AXIS#.SAFEPARAM.SSR_#.VELLOWERLIMIT

Description

Indicates the velocity lower limit of the Safe Speed Range (SSR) safety function.

 

This is n_LL_SSR in the following diagram:

Context

For complete SSR information refer to SSR (Safe Speed Range).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Depends on user units

Range

[-2^31+1, 2^31-1]
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
AXIS1.SAFEPARAM.SSR_1.VELLOWERLIMIT

3161h

09h

Signed32

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_2.VELLOWERLIMIT

3162h

09h

Signed32

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_3.VELLOWERLIMIT

3163h

09h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_1.VELLOWERLIMIT

3261h

09h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_2.VELLOWERLIMIT

3262h

09h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_3.VELLOWERLIMIT

3263h

09h

Signed32

-

-

Read/Write

No